MPC5645S Blinky code please

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5645S Blinky code please

Jump to solution
2,749 Views
peteradamcik
Contributor III

Hi Guys, does anyone have any Assembler or C code to blink a LED on an output port for the MPC5645S?

Please let me know.

Thanks guys

Pete

 

0 Kudos
Reply
1 Solution
2,717 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

here is LED blinking code

For LED conf:

 

  /*  Toggling Red LED D6 on EVB to observe MCU reset event */

  SIU.GPDO[121].R = 0;             /* MPC56x4xS EVB LED: data output: LED on */

  SIU.PCR[121].R = 0x0200;         /* MPC56x4xS/S EVB LED: enable PK[0] as output */

 

  /*  Toggling LED D7 on EVB to observe MCU wakeup event */

  SIU.GPDO[70].R = 0;             /* MPC56x4xS EVB LED: data output: LED on */

  SIU.PCR[70].R = 0x0200;         /* MPC56x4xS/S EVB LED: enable PF[0] as output */

                                                                                                                       

 

Best regards,

Peter

View solution in original post

0 Kudos
Reply
3 Replies
2,718 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

here is LED blinking code

For LED conf:

 

  /*  Toggling Red LED D6 on EVB to observe MCU reset event */

  SIU.GPDO[121].R = 0;             /* MPC56x4xS EVB LED: data output: LED on */

  SIU.PCR[121].R = 0x0200;         /* MPC56x4xS/S EVB LED: enable PK[0] as output */

 

  /*  Toggling LED D7 on EVB to observe MCU wakeup event */

  SIU.GPDO[70].R = 0;             /* MPC56x4xS EVB LED: data output: LED on */

  SIU.PCR[70].R = 0x0200;         /* MPC56x4xS/S EVB LED: enable PF[0] as output */

                                                                                                                       

 

Best regards,

Peter

0 Kudos
Reply
2,735 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have some codes for HVAC or OPEN_VG but those are complex sample codes.

I have asked application team if there is something available. As I do not have the development board here I cant test the code.

However I can write it in case apps dont have one , but not test it here.

Best regards,

Peter

0 Kudos
Reply
2,733 Views
peteradamcik
Contributor III

Hi Peter, yes can you please write some code in assembler or C, that would be very much appreciated.

Just need to set the a port to output and blink a LED via a delay.

Would it be possible for you to write it in Assembler? I'm not to good with C.

Thanks Pete

Peter

 

0 Kudos
Reply