MPC5604E Parallel Data Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604E Parallel Data Interface

1,429 Views
suhass
Contributor II

I have connected 8 Video data lines from Digitizer [P0:7] to MPC5604E, MPC is having 12 Video data lines option VID_D[0:11], as I am using only 8 bit video, I am utilizing only 8 parallel video data lines. The issue is I have not connected P0 - VID_D0, P1-VID_D1, and so on till P7-VID_D7. The connection block diagram is attached please refer.

Will it work?165341_165341.pngpastedImage_1.png

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,355 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, this is OK. There's just one typo - there's missing VID_D4. So, you should use VID_D11 - VID_D4 on MPC5604E.

Regards,

Lukas

0 Kudos
Reply