MPC5604E Parallel Data Interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5604E Parallel Data Interface

1,426件の閲覧回数
suhass
Contributor II

I have connected 8 Video data lines from Digitizer [P0:7] to MPC5604E, MPC is having 12 Video data lines option VID_D[0:11], as I am using only 8 bit video, I am utilizing only 8 parallel video data lines. The issue is I have not connected P0 - VID_D0, P1-VID_D1, and so on till P7-VID_D7. The connection block diagram is attached please refer.

Will it work?165341_165341.pngpastedImage_1.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,352件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, this is OK. There's just one typo - there's missing VID_D4. So, you should use VID_D11 - VID_D4 on MPC5604E.

Regards,

Lukas

0 件の賞賛
返信