CMU CLKMN1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CMU CLKMN1

跳至解决方案
5,053 次查看
Amr_Awny
Contributor II

My first Question:

Shall I configure CMU_3 to monitor the ADC on the max value given in the below table ,and Shall I consider the frequencies below in all CMUs.

Amr_Awny_0-1651009618393.png

 

I did so in the HFREF and LFREF 

=80Mhz*16*4/16Mhz =320

LFREF = 320*0.95 = 304 --> 0x130

HFREF = 320*1.05 = 336 --> 0x150

 if this is correct how shall I test this implementation?

I have added an ADC and tried to change the LFREF and HFREF to other values in order for the CMU to write 1 to CMU_ISR[OLRI] but it failed to do it.

Is there any other configuration to be done?

  • the configuration that I have done
  • CME -> CLKMN1 monitor enable. to 1
  • RCDIV->CLKMT0_RMN division factor. to 11
  • CKSEL1 -> CLKMT0_RMN is selected to 11
  • LFREF = 320*0.95 = 304 --> 0x130

  • HFREF = 320*1.05 = 336 --> 0x150

  •  
0 项奖励
回复
1 解答
4,936 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi

you need to select clock source in MC_CGM.AC0_SC and then enable divider MC_CGM.AC0_DC2 (set DE bit and DIV)

 
 

cgm.png

 

BR, Petr

 

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
5,003 次查看
Amr_Awny
Contributor II

Thank you for your reply, 

I have enabled the MC_CGM_AC0_DC2 divider and read the MC_CGM_AC0=0x0400 0000, however, the CMU_ISR register is fetching the same value written in the CMU_CSR register 

0 项奖励
回复
5,001 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you increase AC0_DC2 divider, will a low reference flag be set?

BR, Petr

0 项奖励
回复
4,907 次查看
Amr_Awny
Contributor II

Yes, it changes, however Now I have another Issue,

In CMU0, CMU3, CMU4 

the ISR of each fire 0x02, FLLI 

What are the values should be written in their division register in order to clear the ISR FLLI bit

 

CMU0

=160Mhz*16*4/16Mhz =640

LFREF = 640*0.95 = 608 --> 0x260

HFREF = 800*1.05 = 672 --> 0x2A0

MC_CGM_AC0_DC0=0x80010000

 

CMU3

=80Mhz*16*4/16Mhz =320

LFREF = 320*0.95 = 304 --> 0x130

HFREF = 320*1.05 = 336 --> 0x150

MC_CGM_AC0_DC2 = 0x80000000

 

CMU4

=80Mhz*16*4/16Mhz =320

LFREF = 320*0.95 = 304 --> 0x130

HFREF = 320*1.05 = 336 --> 0x150

MC_CGM_AC1_DC1= 0x80000000

 

0 项奖励
回复
2,618 次查看
Mennazz
Contributor II
having the same issue @PetrS
0 项奖励
回复
4,958 次查看
Amr_Awny
Contributor II

how to enable the in MC_CGM_AC0 is enabled in MC_ME ?

0 项奖励
回复
4,937 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi

you need to select clock source in MC_CGM.AC0_SC and then enable divider MC_CGM.AC0_DC2 (set DE bit and DIV)

 
 

cgm.png

 

BR, Petr

 

 

0 项奖励
回复
5,032 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

CLKMN0_RMT monitor is only implemented on CMU0, so on CMU3 just LFREF, HFREF and CME can be written, also only  FLL, FHH flags can be set.

Calculation is correct, so be sure selected clock in MC_CGM_AC0 is enabled in MC_ME and MC_CGM_AC0_DC2 divider is enabled. With divider you can also test  low freq reference.

BR, Petr

0 项奖励
回复