AN5374 eTPU config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,803件の閲覧回数
William_Klaus
Contributor II

Hello,

I've been trying to run a code example based on AN5374, but I did not succeed. I can't see any outputs on the pwm pins. The master channel pin is not showing any output either. In the document, it wasn't clear when to call the function "etpu_pwmm_master_irq()". My project is attached below, I used the pwmm API from the cw_etpu website.

Am I missing something?

edit: I've tried the recommendations on this other question but it's still not working.

タグ(1)
0 件の賞賛
返信
1 解決策
1,770件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Have you tried to investigate eTPU registers in the debugger?

Do you have properly setup SIU module for used channels?

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,771件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Have you tried to investigate eTPU registers in the debugger?

Do you have properly setup SIU module for used channels?

0 件の賞賛
返信
1,716件の閲覧回数
William_Klaus
Contributor II

Indeed, the problem was I haven't configured the SIU. Thank you.

0 件の賞賛
返信