******************************************************************************** * Detailed Description: * * Configures the MCANs to transmit and receive a CAN message. * * In this config, MCAN_1 transmits a message. MCAN_2 receives the message. * * MCAN_1 sends message each 1sec. This interval is generated by PIT. * Single TX buffer is used to send n bytes. The message ID is changed for each * transmission. Two standard and 2 extended IDs are sent. * * MCAN_2 is configured to receive a message, SW polling is used. * There are 2 standard and 2 extended ID filter tables defined. Classic filter * configuration is set, means filter ID & mask. * Messages with matched standard ID are received into RXFIFO_0, messages with matched * extended ID then stored in RXFIFO_1. * * EVB connection: * * J37 and J38 to position 1-2 to connect MCAN1 TX/RX to transceiver * * CAN0-CANH on P15-1 to CAN1-CANH on P14-1 * CAN0-CANL on P15-2 to CAN1-CANL on P14-2 * * ------------------------------------------------------------------------------ * Test HW: MPC5777M, MPC57xx Motherboard + MPC5777M_512DS minimodule * Maskset: 0N78H * Target : internal_FLASH * Fsys: 600 MHz PLL1 with 40 MHz crystal reference, * core2 at 200MHz generated from PPL1 * Terminal: None ******************************************************************************** Revision History: 1.0 Jan-5-2017 PetrS Initial Version of MCAN example *******************************************************************************/
查看全文