program a new chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

program a new chip

1,419 Views
Divya28
Contributor I

We are working on a PCB which has following chip MPC8315CVRAFDA. we need to program using a JTAG debugger (LA-7729 JTAG Debugger) with the following script files with the extension .cmm

Is it possible to convert this .cmm to .svf file format(or any other file format which is accepted by this chip?) and upload using normal JTAG developer

Labels (1)
0 Kudos
Reply
1 Reply

1,372 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @Divya28 

Yes, to convert. cmm files to. svf files, you need to use appropriate conversion tools or software. Once you successfully convert the. cmm file to an. svf file, you can use regular JTAG developers to upload it to your chip.

Hope this will help you.

BR

Hang

0 Kudos
Reply