Unable to program MCXN236VNLT custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to program MCXN236VNLT custom board

跳至解决方案
987 次查看
sstcor
Contributor II

Designed a PCB based on the MCXN236VNLT and am trying to program the board using an MCU-Link debug probe, but I am getting the following error.

LinkFlash tool outputLinkFlash tool output

 

标签 (2)
0 项奖励
回复
1 解答
958 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sstcor 

 

Please review the ​FRDM-MCXN236 board schematic and verify your hardware design, particularly the ​SWD interface and ​power circuitry.

https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN236  

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
3 回复数
959 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sstcor 

 

Please review the ​FRDM-MCXN236 board schematic and verify your hardware design, particularly the ​SWD interface and ​power circuitry.

https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN236  

 

BR

Alice

0 项奖励
回复
939 次查看
sstcor
Contributor II

Hi @Alice_Yang ,

After reviewing the schematic, I noticed VDD_SYS on the board is outputting ~3.2V and the datasheet says it should be between 1.71-1.98 V. It's floating in the schematic. Is it normal on 100 pin package?

I have connected the following pins to MCU-Link.

MCU-LinkNXP MCXN236
VTarget3.3V
GNDGND
SWDIOSWDIO
SWCLKSWCLK
RESETRESET

 

Multimeter readings: VDD_MCU = 3.3 V, VCore = 1 V

satinder1_0-1743522807741.png

satinder1_1-1743522824235.png

 

0 项奖励
回复
917 次查看
sstcor
Contributor II
Issue resolved. Missing a 2.2uF capacitor on VDD_SYS pin.
0 项奖励
回复