Unable to program MCXN236VNLT custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to program MCXN236VNLT custom board

ソリューションへジャンプ
991件の閲覧回数
sstcor
Contributor II

Designed a PCB based on the MCXN236VNLT and am trying to program the board using an MCU-Link debug probe, but I am getting the following error.

LinkFlash tool outputLinkFlash tool output

 

ラベル(2)
0 件の賞賛
返信
1 解決策
962件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sstcor 

 

Please review the ​FRDM-MCXN236 board schematic and verify your hardware design, particularly the ​SWD interface and ​power circuitry.

https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN236  

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
963件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sstcor 

 

Please review the ​FRDM-MCXN236 board schematic and verify your hardware design, particularly the ​SWD interface and ​power circuitry.

https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-MCXN236  

 

BR

Alice

0 件の賞賛
返信
943件の閲覧回数
sstcor
Contributor II

Hi @Alice_Yang ,

After reviewing the schematic, I noticed VDD_SYS on the board is outputting ~3.2V and the datasheet says it should be between 1.71-1.98 V. It's floating in the schematic. Is it normal on 100 pin package?

I have connected the following pins to MCU-Link.

MCU-LinkNXP MCXN236
VTarget3.3V
GNDGND
SWDIOSWDIO
SWCLKSWCLK
RESETRESET

 

Multimeter readings: VDD_MCU = 3.3 V, VCore = 1 V

satinder1_0-1743522807741.png

satinder1_1-1743522824235.png

 

0 件の賞賛
返信
921件の閲覧回数
sstcor
Contributor II
Issue resolved. Missing a 2.2uF capacitor on VDD_SYS pin.
0 件の賞賛
返信