NXP MCU RT1166 - How to store data into Internal Flash using JTAG/SWD tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP MCU RT1166 - How to store data into Internal Flash using JTAG/SWD tool

1,439件の閲覧回数
OliveiraKolNxp
Contributor II

Hi,

I need to store data using JTAG into Internal flash memory. I´m able to store them using JTAG/SWD tool ARM J-Link on External Flash Memory connected at FlexSPI1 and it is accessed by address 0x30000000.   IA told me that the access to Internal Flash is 0x600000 but when i try to store any data on it region it return error.

Oliveira
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,363件の閲覧回数
OliveiraKOL
Contributor I

You are correct,

The RT1166 has no Internal Flash to store data. NXP also gave me the same answare.

The Microcontroller of this familly that has 4MBytes of Internal Flash is RT1064.

 

Thanks,

 

Oliveira

0 件の賞賛
返信

1,414件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @OliveiraKolNxp ,

Thanks for your interest in NXP MIMXRT series!

As far as I know, the RT1166 doesn't have internal flash. Please help me to check out chapter 3 of the RM:

Gavin_Jia_0-1739520428452.png

 

Best regards,
Gavin

0 件の賞賛
返信