I am trying to increase the RAM on the board that we are using. We are using the RT1176DVMAA crossover MCU and have 2 parallel Winbond 256Mbit SDRAM ICs currently hooked up. We are looking for much more RAM and need to change out the chip.
I was wondering, since the RT1176 uses the SEMC architecture for interfacing and controlling external SDRAM, would I be able to hook up DDR3 or DDR4 SDRAM chips to this micro instead? I want to avoid using a differential clock for the sake of simplicity AND i want to exhaust the maximum bus width allowable on the 1176, which is 32 bits. I dont mind having two memory ICs, like what we have now, that each have 16bit interfaces. I am looking for an easy replaceable solution that can get me at least 512MB, not Mb, worth of memory for my application purposes that directly interfaces with this micro?
Any advice or help? GPT says that the SEMC on the RT1176 can only support up to DDR2, but I think its either hillucinating or simply doesnt have the right information. DDR2 is a pretty old technology and the RT1176 is a relatively new chip. I would imagine that the RT1176 can interface with newer, better, more available RAM architectures yes?
Please feel free to offer up some alternative chips that would 100% be verified to work and be compatible with this micro:)