MCXC and EEPROM emulation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCXC and EEPROM emulation

ソリューションへジャンプ
1,039件の閲覧回数
pepoja
Contributor II

Hi there,
Please, Is able to use internal FLASH memory in the MCXC242 as a emulated EEPROM/Non-Volatile Memory for store users application settings (few bytes) during running application?
In some LPC microcontrollers is API for In-Application programming which make it possible. How about MCXC242?
Or one and only way is to connect external EEPROM?

Thanks.
Regards,
Peter

ラベル(1)
0 件の賞賛
返信
1 解決策
979件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @pepoja 

If you mean software emulate EEPROM, yes, mcxc242 supports emulated EEPROM.

You can refer to: https://www.nxp.com.cn/docs/en/application-note/AN13542.pdf 

 

BR

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
980件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @pepoja 

If you mean software emulate EEPROM, yes, mcxc242 supports emulated EEPROM.

You can refer to: https://www.nxp.com.cn/docs/en/application-note/AN13542.pdf 

 

BR

Alice

0 件の賞賛
返信