MCXC and EEPROM emulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXC and EEPROM emulation

Jump to solution
1,987 Views
pepoja
Contributor II

Hi there,
Please, Is able to use internal FLASH memory in the MCXC242 as a emulated EEPROM/Non-Volatile Memory for store users application settings (few bytes) during running application?
In some LPC microcontrollers is API for In-Application programming which make it possible. How about MCXC242?
Or one and only way is to connect external EEPROM?

Thanks.
Regards,
Peter

Labels (1)
0 Kudos
Reply
1 Solution
1,927 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @pepoja 

If you mean software emulate EEPROM, yes, mcxc242 supports emulated EEPROM.

You can refer to: https://www.nxp.com.cn/docs/en/application-note/AN13542.pdf 

 

BR

Alice

View solution in original post

0 Kudos
Reply
1 Reply
1,928 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @pepoja 

If you mean software emulate EEPROM, yes, mcxc242 supports emulated EEPROM.

You can refer to: https://www.nxp.com.cn/docs/en/application-note/AN13542.pdf 

 

BR

Alice

0 Kudos
Reply