MCUXpresso Tools don´t support MCX A processor peripherals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso Tools don´t support MCX A processor peripherals

跳至解决方案
1,605 次查看
berndgrossmann
Contributor II

I need a PWM on Pin 3.1 on MCX A153 processor.

In the config tool I can select this processor but most peripherals are not supported.

Example eFlexPWM: PWM driver is not found in the toolchain.

Is ther a way to add these drivers to the toolchain?

标签 (1)
0 项奖励
回复
1 解答
1,531 次查看
berndgrossmann
Contributor II

berndgrossmann_0-1731054819216.png

The solution is to go to Manage SDK components and select PWM SDK driver.

berndgrossmann_1-1731054913606.png

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,587 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your question, but this is not enough clear, "PWM driver is not found in the toolchain".

If you are using the MCUXpresso need to select all the libraires and the toolchain.

Pavel_Hernandez_0-1730744079640.png

Then when you have installed on the IDE you could import some examples from that like this.

Pavel_Hernandez_1-1730744161079.png

Best regards,
Pavel

0 项奖励
回复
1,532 次查看
berndgrossmann
Contributor II

berndgrossmann_0-1731054819216.png

The solution is to go to Manage SDK components and select PWM SDK driver.

berndgrossmann_1-1731054913606.png

 

 

0 项奖励
回复
1,517 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the next information could help you.

I opened a blnky_led example where there is not any a PWM, so I select the MCUXpresso Configuration then on the pop-up window and type PWM.

破坏者
Pavel_Hernandez_0-1731105011048.pngPavel_Hernandez_2-1731105056522.png

Pavel_Hernandez_3-1731105113743.png

Pavel_Hernandez_4-1731105153973.png

Let me know if the information is not helpful maybe I do not understand.

Best regards,
Pavel

0 项奖励
回复
1,466 次查看
berndgrossmann
Contributor II
I posted the solution above
0 项奖励
回复