MCUXpresso Tools don´t support MCX A processor peripherals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Tools don´t support MCX A processor peripherals

Jump to solution
1,592 Views
berndgrossmann
Contributor II

I need a PWM on Pin 3.1 on MCX A153 processor.

In the config tool I can select this processor but most peripherals are not supported.

Example eFlexPWM: PWM driver is not found in the toolchain.

Is ther a way to add these drivers to the toolchain?

Labels (1)
0 Kudos
Reply
1 Solution
1,518 Views
berndgrossmann
Contributor II

berndgrossmann_0-1731054819216.png

The solution is to go to Manage SDK components and select PWM SDK driver.

berndgrossmann_1-1731054913606.png

 

 

View solution in original post

0 Kudos
Reply
4 Replies
1,574 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your question, but this is not enough clear, "PWM driver is not found in the toolchain".

If you are using the MCUXpresso need to select all the libraires and the toolchain.

Pavel_Hernandez_0-1730744079640.png

Then when you have installed on the IDE you could import some examples from that like this.

Pavel_Hernandez_1-1730744161079.png

Best regards,
Pavel

0 Kudos
Reply
1,519 Views
berndgrossmann
Contributor II

berndgrossmann_0-1731054819216.png

The solution is to go to Manage SDK components and select PWM SDK driver.

berndgrossmann_1-1731054913606.png

 

 

0 Kudos
Reply
1,504 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the next information could help you.

I opened a blnky_led example where there is not any a PWM, so I select the MCUXpresso Configuration then on the pop-up window and type PWM.

Spoiler
Pavel_Hernandez_0-1731105011048.pngPavel_Hernandez_2-1731105056522.png

Pavel_Hernandez_3-1731105113743.png

Pavel_Hernandez_4-1731105153973.png

Let me know if the information is not helpful maybe I do not understand.

Best regards,
Pavel

0 Kudos
Reply
1,453 Views
berndgrossmann
Contributor II
I posted the solution above
0 Kudos
Reply