MCIMX6Q5EYM10AE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q5EYM10AE

2,677 Views
RamakrishnaC
Contributor III

Hi Team,

Below i have mentioned net names. how much current is required for each net? Please share the details. It is not mentioned any documents i have verified. please help me.

NVCC_EIM3.3VD
NVCC_GPIO3.3VD
NVCC_LCD3.3VD
NVCC_JTAG3.3VD
NVCC_ENET2.5VD
NVCC_RGMII2.5VD
NVCC_MIPI2.5VD
NVCC_LVDS2.5VD

 

Thank you.

Labels (1)
5 Replies

2,578 Views
pengyong_zhang
NXP Employee
NXP Employee
0 Kudos
Reply

2,604 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @RamakrishnaC 

What do you mean "the individual maximum requirement current details "?

B.R

0 Kudos
Reply

2,591 Views
RamakrishnaC
Contributor III

Hi,

Thanks for reply.

Below i am giving explanation of  individual maximum requirement current details maens.

i.MX 6Quad and 6Dual chips can support three
different EIM power rail voltage levels:

NVCC_EIM0(K19),

NVCC_EIM1(L19),

NVCC_EIM2(M19).

Is these pins are input or Output. If input means What is the voltage and current requirements?

This is what i am asking for previous message mentioned signals as well..

Thank you.

0 Kudos
Reply

2,650 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @RamakrishnaC 

You can get the value from the below link HDG file.

https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG

B.R

0 Kudos
Reply

2,644 Views
RamakrishnaC
Contributor III

Hi,

Thank you.

In this document showing Supply regulator current capability group of nets. already verified this document. Could please share the individual maximum requirement current details? 

RamakrishnaC_1-1725000711410.png

RamakrishnaC_2-1725000767028.png

Thanks & Regards