MCIMX6Q5EYM10AE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6Q5EYM10AE

2,714件の閲覧回数
RamakrishnaC
Contributor III

Hi Team,

Below i have mentioned net names. how much current is required for each net? Please share the details. It is not mentioned any documents i have verified. please help me.

NVCC_EIM3.3VD
NVCC_GPIO3.3VD
NVCC_LCD3.3VD
NVCC_JTAG3.3VD
NVCC_ENET2.5VD
NVCC_RGMII2.5VD
NVCC_MIPI2.5VD
NVCC_LVDS2.5VD

 

Thank you.

ラベル(1)
5 返答(返信)

2,615件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee
0 件の賞賛
返信

2,641件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

hi @RamakrishnaC 

What do you mean "the individual maximum requirement current details "?

B.R

0 件の賞賛
返信

2,628件の閲覧回数
RamakrishnaC
Contributor III

Hi,

Thanks for reply.

Below i am giving explanation of  individual maximum requirement current details maens.

i.MX 6Quad and 6Dual chips can support three
different EIM power rail voltage levels:

NVCC_EIM0(K19),

NVCC_EIM1(L19),

NVCC_EIM2(M19).

Is these pins are input or Output. If input means What is the voltage and current requirements?

This is what i am asking for previous message mentioned signals as well..

Thank you.

0 件の賞賛
返信

2,687件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

HI @RamakrishnaC 

You can get the value from the below link HDG file.

https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG

B.R

0 件の賞賛
返信

2,681件の閲覧回数
RamakrishnaC
Contributor III

Hi,

Thank you.

In this document showing Supply regulator current capability group of nets. already verified this document. Could please share the individual maximum requirement current details? 

RamakrishnaC_1-1725000711410.png

RamakrishnaC_2-1725000767028.png

Thanks & Regards