Dear Kevin,
the difference in the voltage between the channels can be because of active balancing. Please see below an answer to another customer experiencing voltage change (raise and drop) during one channel balancing.
DESCRIPTION
This behavior is typical of a serial resistance in the cell terminals. If a load is applied on cell2 through the cell terminals (such as bell balancing for example), it will generate a voltage drop on the line. Since cell3 measurement utilizes the same cell terminal, the same drop will be observed on cell3, but on the opposite direction and typically half the magnitude.
If the load is applied to the whole battery pack (via the power negative and positive battery terminals), you should not observe this behavior.
In a nutshell, to avoid this behavior, either reduce cell terminal resistance or reduce the load current.
With Best Regards,
Jozef