MCXA153VLF external crystal oscillator configuration.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCXA153VLF external crystal oscillator configuration.

Jump to solution
1,893 Views
bogdanurbanczyk
Contributor II

Hello,
MCXC44X Sub-Family Reference Manual (page 461) describes external crystal (or resonator) connections. Are 3 type of configuratons (Connection 1 to Connection 3).
Why MCXA153 Reference Manual hasn't any informations of external crystal and capacitors configuratons?
In FRDM-MCXA153 schematic is connection with 18pF capacitors and 8MHz crystal.
best regards
Bogdan

 

Labels (1)
0 Kudos
Reply
1 Solution
1,798 Views
bogdanurbanczyk
Contributor II

Hello Habib,
I understand that NXP recommends using FIRC with trim capability. I accept this. I will try connecting an external crystal according to the FRDM-MCXA153 schematic.
best regards
Bogdan

View solution in original post

0 Kudos
Reply
4 Replies
1,799 Views
bogdanurbanczyk
Contributor II

Hello Habib,
I understand that NXP recommends using FIRC with trim capability. I accept this. I will try connecting an external crystal according to the FRDM-MCXA153 schematic.
best regards
Bogdan

0 Kudos
Reply
1,848 Views
bogdanurbanczyk
Contributor II

Hello Habib,
Your answer was about the MCX C44X processor.
I need information on how to connect an external crystal (or resonator) to the MCXA153 microcontroller.
The MCXAP64M96FS3RM.pdf and MCXAP64M96FS3.pdf files do not contain any information about connecting an external crystal or capacitors.

best regards
Bogdan

 

0 Kudos
Reply
1,837 Views
Habib_MS
NXP Employee
NXP Employee

Hello @bogdanurbanczyk,

Apologies for the confusion.
For detailed information regarding the external crystal and load capacitors, please refer to Section 4.2, "Clock Modules" in the datasheet. This section outlines the crystal specifications as well as the recommended capacitance values based on the crystal frequency.

Habib_MS_0-1753901407829.png

BR
Habib

0 Kudos
Reply
1,860 Views
Habib_MS
NXP Employee
NXP Employee

Hello @bogdanurbanczyk,
You can find the oscillator frequency specifications for the crystal in Section 3.3.2.2 of the datasheet. Additionally, the section you mentioned includes a table that outlines the supported crystal frequency ranges and the different connection options available, depending on your application:

Habib_MS_0-1753821802802.png

On the other hand, the load capacitor values should follow the crystal or resonator manufacturer's recommendations, as referenced in Table 20: "Oscillator DC Electrical Specifications" of the datasheet. Please keep the following recommendations in mind:

  • If the load capacitors (Cx, Cy) are greater than 30 pF, use Connection 3.
  • When using the low-frequency oscillator (RANGE = 00), the integrated capacitors can provide Cx and Cy.

BR
Habib

0 Kudos
Reply