Is there an driver example for the Edgelock Secure Subsystem (ELS) on the MCXN947?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an driver example for the Edgelock Secure Subsystem (ELS) on the MCXN947?

Jump to solution
824 Views
ClarkS
Contributor III

I have searched the driver_examples in SDK_25_03_00 and do not find an example for using the ELS. Will one be available soon? 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
771 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @ClarkS ,

Thanks for your post.  We already have the ELS demos in SDK, please refer to the attached picture.

 

BRs,

Celeste

 

-------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
7 Replies
609 Views
ClarkS
Contributor III

It's not clear to me how to configure the SDK Builder but based on my understanding of it, the ELS examples are apparently available for the MCUXpresso IDE and not for the VSCode Extension. Am I correct? Why is that?

0 Kudos
Reply
607 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello, @ClarkS 

The SDK builder is where you can download the SDK. ELS examples also exist in the VSCode Extension.

Celeste_Liu_0-1754362500580.png

 

BRs,

Celeste

0 Kudos
Reply
589 Views
ClarkS
Contributor III

I think I’m beginning to understand the SDK Builder. This time I picked so crypto related middleware, VSCode, macOS and got SDK_25.06.00_MCXN947 

When we select several items in the filter, am I correct that it’s not building and sdk with only those items. Instead it’s only going to select a prebuilt SDK that has at least those items plus you get whatever more is in it. On the other hand I’ve seen if you select certain things, it may only offer an older SDK, but then it shows you what you could remove to get the newest SDK. Pretty nice.

I'm still confused on filtering on middleware vs examples. If I filter on ELS middleware only, the SDK will also probably contain examples. Correct?

Or if I filter on the ELS examples, it will certainly contain the middleware, and it will contain all the examples, even it it only lets me select one example. Correct?

it only lets me pick one ELS example but I assume that’s because when you select one you automatically get them all. 

Is there any instructions on using the SDK Builder!

Thank you for your help!

Clark

 

0 Kudos
Reply
567 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @ClarkS ,

Normally, when downloading the SDK, I will directly select all the middleware.
Of course, if you only need the ELS demo, you can also select only "ELS" in the middleware section.

Regarding the use of SDK Builder, the attachments in the following link may be helpful to you.

Hands-On Workshop: Using MCUXpresso SDK - NXP Community

In addition, if you have any new questions, please feel free to create a new post.

BRs,

Celeste

0 Kudos
Reply
760 Views
ClarkS
Contributor III

I’m still not sure where these examples are located, but I’ll find them and probably learn about how your SDKs are organized in the process. Thank you!

0 Kudos
Reply
702 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello , you can find our SDK here: Select Board | MCUXpresso SDK Builder

Celeste_Liu_0-1753773873731.png

 

Which IDE are you using? We support below Toolchain/IDE:

Celeste_Liu_1-1753773915880.png

 

0 Kudos
Reply
772 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @ClarkS ,

Thanks for your post.  We already have the ELS demos in SDK, please refer to the attached picture.

 

BRs,

Celeste

 

-------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply