Dockerize MCUXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dockerize MCUXpresso

跳至解决方案
1,710 次查看
erikraynolds
Contributor IV

Is there. Docker file for MCUXpresso development available.

can be run mcuxpresso from within a Docker under WSL2?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,681 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @erikraynolds ,

There is currently no official Dockerfile provided for MCUXpresso development. However, in my opinion, it is feasible to run MCUXpresso within a Docker under WSL2, but you need to develop it on your own. You can refer to the following link:

GitHub - aduskett/docker-mcuxpresso: Run mcuexpresso in a docker container with X11 forwarding

GitHub - snhobbs/MCUXpressoDocker: Docker script for setting up MCUXpresso

Hope the above information is helpful to you.

BRs,

Celeste

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,682 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @erikraynolds ,

There is currently no official Dockerfile provided for MCUXpresso development. However, in my opinion, it is feasible to run MCUXpresso within a Docker under WSL2, but you need to develop it on your own. You can refer to the following link:

GitHub - aduskett/docker-mcuxpresso: Run mcuexpresso in a docker container with X11 forwarding

GitHub - snhobbs/MCUXpressoDocker: Docker script for setting up MCUXpresso

Hope the above information is helpful to you.

BRs,

Celeste

0 项奖励
回复