MCX C SERIES PROGRAMMER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCX C SERIES PROGRAMMER

1,622 Views
RACHIT_JUTHANI
Contributor I

HI I would like to understand if I am using MCX C SERIES then how to program the MCU . What programmer do I have to use? And for MCX N/A/W  do I have to change the programmer or same can be used. I am asking for a mass manufacturing and also for proto testing .

Thank you.

0 Kudos
Reply
1 Reply

1,573 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @RACHIT_JUTHANI ,

Thanks for contacting NXP Tech Support. Apologies for the late reply. For mass manufacturing, we more strongly recommend using PEmicro Cyclone programmers/PEmicro Cyclone FX programmer. The page for NXP products they support is as follows: PEmicro Partners . There, you can see all of the MCX A/C/N/W devices. MCX C and W are listed in the wrong category under Kinetis.

Regarding the selection of PEmicro programmers, you can contact PEmicro support. We hope the above information is helpful to you.

Best Regards

Celeste

0 Kudos
Reply