MCX Microcontrollers Knowledge Base

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCX Microcontrollers Knowledge Base

讨论

排序依据:
The Serial Peripheral Interface (SPI) is ubiquitous in embedded systems for interfacing to external peripherals such flash memories, EEPROMs, analog to digital converters and sensors. SPI controllers are essentially shift registers. When combined with DMA, SPI can be used for interesting use cases. In this paper we will look at an LED lighting application and hint at some other interesting use cases such as PDM audio streams.
查看全文
The NXP MCXA153 is a useful microcontroller for small, embedded USB devices. Combined with the USB stack built into the SDK, or with the open source TinyUSB stack,  it is easy to creak your own USB protocol bridges and test tools. In this paper we showed to how to integrate TinyUSB into an MCUXpresso project and demonstrated  with a USB CDC / WebUSB application for a BLDC Motor controller test application.
查看全文
Device manufacturers spend months or years developing application software for their end products, which is one of the most valuable assets.   During the software development phase, the engineering teams use development platforms with easy access to critical electronics development components, but this is no longer the case when the projects move to the manufacturing phase. Once the project is ready to go to manufacturing the exposure of the electronics components changes drastically from a development environment. In Most cases the programming connector is not accessible because PCB now resides inside an assembled enclosure or has been removed to reduce PCB cost or very important, for security reasons. On Any case you still need to download manufacture testing FW or final product firmware to the microcontrollers in the system and to help with that NXP MCX microcontrollers have embedded tools called the In-system programming to assist with the FW provisioning. In-System programming (ISP) is a method of erasing and programing the on-chip FLASH or RAM memory using a ROM bootloader firmware without using an external Debug tool. NXP MCX Microcontroller family have ISP support over several serial peripherals like: UART SPI I2C USB High-Speed USB Full-Speed CAN Depending on the MCX microcontroller you are using the ISP supported peripherals will change so it is important to review the “In-system Programming” reference manual chapter on the specific MCX microcontroller that will be used. One important thing to remark is that the ISP firmware resides inside a ROM section on the MCX microcontrollers, meaning that the entire flash of the device can be used for the main application without the need of reserving on-chip FLASH for a firmware provisioning bootloader. The flash bootloader code is executed automatically every time the part is powered on or reset. The bootloader can execute the ISP command handler or pass execution to the user application code depending on several conditions. When the internal flash in empty the MCX microcontroller automatically enters ISP mode. Translating this to the manufacturing, Microcontrollers are ready to get firmware using ISP after the PCB assembly process. In-circuit programming features can be tested using any FRDM or EVK boards available for MCX family. You can find instructions of how to use the ISP mode alongside many other MCX examples, demos and tools directly on NXP Application Code Hub   Here are some Application Code Hub for ISP on MCX FRDM boards: How to use In-System Programming (ISP) on FRDM-MCXN947 How to use In-System Programming (ISP) on FRDM-MCXA153   Security is at the core of NXP. Not only do we want each element of our devices or software to be safe and secure, but it is just as critical that we enable the manufacturing of each customer's product to be secure. Manufacturing processes should be worry-free and hassle-free with the backing of highly secure technology, even if the manufacturing site itself cannot provide strong assurances of security. NXP is offers a variety of features that enable OEMs to protect their IP and revenue. Utilizing our MCUXpresso Secure Provisioning tool (SEC) and Secure Provisioning SDK (SPSDK)   MCXpresso Secure Provisioning tool (SEC) The MCUXpresso Secure Provisioning tool (SEC) is a GUI-based application that provides firmware provisioning operations such as setting up e-fuses/OTP, building secure boot image, flash programming, keys generation, trust provisioning, etc.   NXP SEC tool features: Easy-to-use configuration of secure provisioning project settings Enables direct communication with attached device for provisioning and programming. Supports generation of executable scripts for production use Manufacturing mode for simplified production line use     Secure Provisioning SDK (SPSDK) Secure Provisioning SDK (SPSDK) is an open-source development kit with its source code released on Github and PyPI. It contains a set of API modules for custom production tool development which requires more advanced secure provisioning flow. SPSDK enables connection and communication with NXP’s microcontrollers for the following purposes:   Generation of Secure Binary (SB) bootable images Security features configuration (CMPA, CFPA, Trustzone, secure bootloader, debug authentication, etc.) Generation and management of cryptographic keys and certificates Trust provisioning and secure programming through MCU Bootloader Debug authentication through J-Link, PEmicro and PyOCD debug probes   For more information about NXP development ecosystem for microcontrollers please visit: MCUXpresso Suite of Software and Tools https://nxp.com/mcuxpresso  
查看全文
Developing code for MCXN family from Scratch The MCX family is a newly released MCU family, of course, the SDK package includes almost all the examples of the MCXN modules based on the SDK driver, for example led_blinky which shows the method of toggling GPIO, CTimer interrupt, etc. While the program in this article doesn’t use SDK driver. It focuses on understanding the related module from register level which is friendly to beginners to understand MCX working mechanism. The doc introduces how to toggle a GPIO, how to have CTimer generate interrupt, and in the CTimer ISR, toggle a LED, while it also describes how to initialize the NVIC so that CTimer can generate ISR by writing the module registers without calling the SDK driver. Environment: FRDM-MCXN947 board MCUXPresso IDE v11.9.0 IDE on Win10 OS   1. Toggle a LED On the FRDM-MCXN947 board, the PIO0_10(P0_10) of MCXN947 is connected to a LED. With MCUXPresso IDE with v11.9.0, you can add the code to test the LED toggling and CTimer interrupt function.   1.1 Configure the PIO0_10 pin as GPIO0_10 pin SYSCON->AHBCLKCTRLSET[0]=1<<13; PORT0->PCR[10]=0x1000; Before you initialize the PORT0 register to assign the PIO0_10 function, you have to enable the PORT0 gated clock in the SYSCON->AHBCLKCTRL0 reg. Write the PORT0->PCR[10]=0x1000; to configure the PIO0_10 as GPIO0_10 function. 1.2 Configure the GPIO0_10 pin as GPIO output mode and toggle the GPIO pin. SYSCON->AHBCLKCTRLSET[0]=1<<19; GPIO0->PDDR|=1<<10; GPIO0->PTOR=1<<10; Before you initialize the GPIO0 registers, you have to enable the GPIO0 gated clock in the SYSCON->AHBCLKCTRL0 reg. Set the bit 10 of GPIO0->PDDR so that the GPIO0_10 is in GPIO output mode. Toggle GPIO0_10 pin by writing the bit 10 in GPIO0->PTOR reg   Set a break point in the debugger on the GPIO0->PTOR=1<<10; line,and run step by step, you can see that led toggles.   2. Initialize CTimer 2.1 enable Ctimer gated clock and clock source and divider. Before you initialize the CTimer register, you have to enable the CTimer gated clock. For example, enable CTimer4 gated clock with the line: SYSCON->AHBCLKCTRLSET[2]=1<<22; You have to also select the CTimer clock source and Ctimer clock divider. For example, set the CTimer4 clock source and divider. SYSCON->CTIMERCLKSEL[4]=0x04; SYSCON->CTIMERCLKDIV[4]=0x02; //P0_10 is LED red void GPIOInit(void) { SYSCON->AHBCLKCTRLSET[0]=1<<13; PORT0->PCR[10]=0x1000; //enable gated clock of GPIO SYSCON->AHBCLKCTRLSET[0]=1<<19; GPIO0->PDDR|=1<<10; GPIO0->PTOR=1<<10; //set break point here GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; } 2.2 Initialize the CTimer register. CTIMER4->CTCR=0x00; CTIMER4->PR=0x00; //set the CTimet4 mode and enable interrupt for match0 CTIMER4->MCR=0x03; CTIMER4->PWMC=0x00; //set the CTimer4 cycle time CTIMER4->MR[0]=2000000; CTIMER4->MSR[0]=2000000; //Start up CTimer4 CTIMER4->TCR=0x01; 2.3 Initialize the NVIC The IRQ number of CTimer4 is 56, so you have to set the bit 24 of both NVIC->ISER[1]|=1<<24; NVIC->ICPR[1]|=1<<24; and set the priority of NVIC->IPR[56] with 0x00; NVIC->IPR[56]=0x00;   //CTimer4 IRQ 56, 56-32=24 void cTimer0Init(void) { //CLOCK_SetClkDiv(kCLOCK_DivCtimer4Clk, 1u); //CLOCK_AttachClk(kFRO_HF_to_CTIMER4); //enable Ctimer4 gated clock SYSCON->AHBCLKCTRLSET[2]=1<<22; SYSCON->PRESETCTRLSET[2]=1<<22; SYSCON->PRESETCTRLCLR[2]=1<<22; SYSCON->CTIMERGLOBALSTARTEN|=1<<4; //select CTimer4 clock source SYSCON->CTIMERCLKSEL[4]=0x04; SYSCON->CTIMERCLKDIV[4]=0x02; //init the CTimer0 CTIMER4->CTCR=0x00; CTIMER4->PR=0x00; CTIMER4->MCR=0x03; CTIMER4->PWMC=0x00; CTIMER4->MR[0]=2000000; CTIMER4->MSR[0]=2000000; //CTIMER0->IR=0x01; CTIMER4->TCR=0x01; NVIC->ISER[1]|=1<<24; NVIC->ICPR[1]|=1<<24; NVIC->IPR[56]=0x00; } 2.3 Each interrupt source has unique interrupt service routine in the file startup_mcxn947_cm33_core0.c For the CTimer4 ISR, it is called: CTIMER4_IRQHandler So it is okay to fill the function: void CTIMER4_IRQHandler(void) { //clear flag CTIMER4->IR|=0x01; //toggle LED GPIO0->PTOR=1<<10; } In conclusion, the doc gives a snippet which can toggle a LED by writing the register directly. It also give the code to configure CTimer4 so that it can generate interrupt, in the ISR, toggle a LED. Appendix This is the entire source code:   /* * Copyright 2019 NXP * All rights reserved. * * SPDX-License-Identifier: BSD-3-Clause */ #include "pin_mux.h" #include "peripherals.h" #include "board.h" /******************************************************************************* * Definitions ******************************************************************************/ void clockOUTInit(void); void GPIOInit(void); void cTimer0Init(void); void MRTInit(void); /******************************************************************************* * Prototypes ******************************************************************************/ /******************************************************************************* * Variables ******************************************************************************/ /******************************************************************************* * Code ******************************************************************************/ /*! * @brief Main function */ int main(void) { /* Board pin init */ CLOCK_EnableClock(kCLOCK_Gpio0); BOARD_InitPins(); BOARD_BootClockFRO12M(); //FlexPWMPinInit(); GPIOInit(); cTimer0Init(); //MRTInit(); __asm("nop"); while (1) { } } //P0_10 is LED red void GPIOInit(void) { SYSCON->AHBCLKCTRLSET[0]=1<<13; PORT0->PCR[10]=0x1000; //enable gated clock of GPIO SYSCON->AHBCLKCTRLSET[0]=1<<19; GPIO0->PDDR|=1<<10; //set a break point here and run step by step GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; GPIO0->PTOR=1<<10; } //CTimer4 IRQ 56, 56-32=24 void cTimer0Init(void) { // CLOCK_SetClkDiv(kCLOCK_DivCtimer4Clk, 1u); // CLOCK_AttachClk(kFRO_HF_to_CTIMER4); //enable Ctimer4 gated clock SYSCON->AHBCLKCTRLSET[2]=1<<22; SYSCON->PRESETCTRLSET[2]=1<<22; SYSCON->PRESETCTRLCLR[2]=1<<22; SYSCON->CTIMERGLOBALSTARTEN|=1<<4; //select CTimer4 clock source SYSCON->CTIMERCLKSEL[4]=0x04; SYSCON->CTIMERCLKDIV[4]=0x02; //init the CTimer0 CTIMER4->CTCR=0x00; CTIMER4->PR=0x00; CTIMER4->MCR=0x03; CTIMER4->PWMC=0x00; CTIMER4->MR[0]=2000000; CTIMER4->MSR[0]=2000000; //CTIMER0->IR=0x01; CTIMER4->TCR=0x01; NVIC->ISER[1]|=1<<24; NVIC->ICPR[1]|=1<<24; NVIC->IPR[56]=0x00; } void CTIMER4_IRQHandler(void) { //clear flag CTIMER4->IR|=0x01; //toggle LED GPIO0->PTOR=1<<10; } //MRT0 interrupt IRQ is 30 void MRTInit(void) { SYSCON->AHBCLKCTRLSET[1]=1<<0; SYSCON->PRESETCTRLSET[1]=1<<0; SYSCON->PRESETCTRLCLR[1]=1<<0; MRT0->CHANNEL[0].INTVAL=6000000; MRT0->CHANNEL[0].INTVAL|=1<<31; MRT0->CHANNEL[0].CTRL=0x01; NVIC->ISER[0]|=1<<30; NVIC->ICPR[0]|=1<<30; NVIC->IPR[30]=0x00; } void MRT0_IRQHandler(void) { if(MRT0->CHANNEL[0].STAT&0x01) { MRT0->CHANNEL[0].STAT|=0x01; } //toggle LED GPIO0->PTOR=1<<10; }
查看全文
In order to recover your board, you need to accomplish the following: Ensure that your PC successfully enumerates the LinkServer debugger under the COM ports. Confirm that you can attach to the running code on the board. When attempting to program the board, the following error appears:   The device stops during initialization because the value of SIM_CHIPCTL is not set to its default after reset. This happens because SRAMU and SRAML are retained across resets, which causes a flash initialization error. To resolve this issue, modify the debug script to override the SIM_CHIPCTL register with its default value: 0x0030_0000. Locate the file MCXE24x_connect.scp. If you are using the default installation path, it should be located at: C:\NXP\LinkServer_YourVersion\binaries\Scripts   Open the file and add the line "Poke32 this 0x40048004 0x00300000" I recommend do it after the "Release NRESET" message.     Note: You need to add a number to each line of code    After making this change, you should be able to program your MCX E24x board as usual.
查看全文
NXP officially launched the MCX C series chips in July 2024. As a Cortex-M0+ MCU with high cost-effectiveness, energy efficiency, and security, it strongly supports the upgrade of traditional 8-bit and 16-bit designs. Since its release, the chip has gained rapid favor among customers, with many projects now entering mass production. In practical applications, more and more customers have inquired about how to enter the ISP mode of MCX C series chips and complete firmware updates. We have previously introduced the method using the blhost tool (see MCX C: How to Enter the ROM Bootloader to Update the Firmware - NXP Community). It is worth noting that the MCUXpresso Secure Provisioning (SEC) tool now supports MCX C series chips starting from version 25.03. The operation process is described in detail below. Refer to the attached PDF file for details.
查看全文