Debugging app deployed to nor flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging app deployed to nor flash

ソリューションへジャンプ
2,063件の閲覧回数
arunkumar_g
Contributor IV

Hello 

 

I'm using 1189EVK and loaded freertos hello world cm33 app to vscode. 

I want to build, deploy and debug that app. But when deploying vscode shows an error 

"Error: ENOENT: no such file or directory, open 'C:\NXP\MCUX_Provi_v9\bin\deviceInfo.json'" and indeed that file is not in that directory (provisioning tool version is 9.0.1). Is that vscode doen't support debugging on flash?

 

Thanks

 

0 件の賞賛
返信
1 解決策
2,028件の閲覧回数
Melania
NXP Employee
NXP Employee

Hi,

Indeed you can have this problem if no rights, the issue is logged and will be addressed soon. In the mean time, please find attached the deviceInfo file. Remove the txt extension, copy it in the location and let me know if the problem is fixed.

Regards,

Melania.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,029件の閲覧回数
Melania
NXP Employee
NXP Employee

Hi,

Indeed you can have this problem if no rights, the issue is logged and will be addressed soon. In the mean time, please find attached the deviceInfo file. Remove the txt extension, copy it in the location and let me know if the problem is fixed.

Regards,

Melania.

0 件の賞賛
返信