Debugging app deployed to nor flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging app deployed to nor flash

Jump to solution
3,488 Views
arunkumar_g
Contributor IV

Hello 

 

I'm using 1189EVK and loaded freertos hello world cm33 app to vscode. 

I want to build, deploy and debug that app. But when deploying vscode shows an error 

"Error: ENOENT: no such file or directory, open 'C:\NXP\MCUX_Provi_v9\bin\deviceInfo.json'" and indeed that file is not in that directory (provisioning tool version is 9.0.1). Is that vscode doen't support debugging on flash?

 

Thanks

 

0 Kudos
Reply
1 Solution
3,453 Views
Melania
NXP Employee
NXP Employee

Hi,

Indeed you can have this problem if no rights, the issue is logged and will be addressed soon. In the mean time, please find attached the deviceInfo file. Remove the txt extension, copy it in the location and let me know if the problem is fixed.

Regards,

Melania.

View solution in original post

0 Kudos
Reply
1 Reply
3,454 Views
Melania
NXP Employee
NXP Employee

Hi,

Indeed you can have this problem if no rights, the issue is logged and will be addressed soon. In the mean time, please find attached the deviceInfo file. Remove the txt extension, copy it in the location and let me know if the problem is fixed.

Regards,

Melania.

0 Kudos
Reply