MCUXpresso Training Hub

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Training Hub

Discussions

Sort by:
Documentation Open-CMSIS-Packs Documentation    This training currently covers the following areas: Getting started - Installation and environment setup Build, Flash, and Debug Using partner packs - EmSA walkthrough Using partner packs - Crank Software walkthrough 
View full article
Open-CMSIS-Pack project  This is a link to the Open-CMSIS-Pack project website. This resource provides all the technical details behind CMSIS-Packs.   Working with Open-CMSIS-Packs  This is a link to documentation for MCUXpresso for VS Code that shows the user how to get started with Open-CMSIS-Packs.      
View full article
GOAL Learn how to import CMSIS packs into existing projects. In this particular project, CMSIS packs from EmSA will be used alongside the lpcxpresso55s16_mcan_interrupt_transfer example obtained from the LPCXpresso55s16 SDK.   ENVIRONMENT This guide requires MCUXpresso IDE v11.9.1 or latest.   PROCEDURE 1. Import the lpcxpresso55s16_mcan_interrupt_transfer example into the workspace. In this example, SDK drivers, startup and board interface files are readily available. CAN pins are already routed and enabled.     2. Launch Config Tools to configure the clock for the CAN peripheral     3. Configure the clock for the CAN peripheral. I. Set up the main clock so that it is generated from crystal or oscillator, and it is evenly dividable by 40 MHz.   II. Change the PLL configuration an even multiple of 40 MHz   III. Set the CAN divider to get a 40 MHz clock.   4. Update the code.   5. Add Open-CMSIS Packs to the project.   6. Project set-up I. Add the watchdog driver.   II. Exclude the fsl_mcan.c module from the build. A dedicated version is included in the EmSA packs.   III. Add the main.c module from CMSIS template   IV. Exclude or remove the original main source code mcan_interrupt_transfer.c file.   7. Save and build the project.          
View full article
GOAL Learn how to import CMSIS packs into existing projects. In this particular project, CMSIS packs from Crank will be used alongside the freertos_hello example obtained from the MIMXRT1060-EVKB SDK. Note: This walkthrough was adapted from Crank Software's guide included with their CMSIS Pack.   ENVIRONMENT This guide requires MCUXpresso IDE v11.9.1 or latest. MIMXRT1060-EVK SDK version 2.16 or latest.   PROCEDURE 1. Import the freertos_hello example into the workspace. Be sure to set the library type to Newlib (semihost).     2. Rename the project to freertos_sbengine.     3. Add drivers to the project. Right click on the project and select SDK Management -> Manage SDK Components. NOTE: Select Keep Existing and do not replace the FreeRTOSConfig.h file when prompted after adding the following components: Under Drivers -> Device -> SDK Drivers, select: cache elcdif pxp Under Board Components -> Device -> SDK Drivers, select: ft5406_rt Under Software Components -> Device -> SDK Drivers, select: video-common     4. Add additional components to the project. Add the gt911 driver if required by your display. This driver can be found in the MIMXRT1060-EVKB SDK.   Navigate to components/gt911:   Copy the fsl_gt911.c and fsl_gt911.h into the touchpanel directory in the project:     Change the memory manager configuration from the default used by FreeRTOS.   Remove the heap_4.c from the project folder. This is found in freertos/freertos-kernel/portable/MemMang.   Add the heap_3.c into the project folder freertos/FreeRTOS/portable/MemMang. This file can be found in the MIMXRT1060-EVKB SDK.     5. Download the Crank Software pack from Arm Keil | CMSIS Packs.     6. Import the Crank Software pack into MCUXpresso IDE.       7. The Crank Software pack is a graphics bundle that contains six components: Board Display Memory Runtime Libraries Runtime Source Task For this walkthrough, we will add all the components except the Runtime Source component. This component is intended for custom changes. To add the components, right click on the project and select SDK Management -> Add Open-CMSIS Components: Once the components are selected press Ctrl + s to save the components in the project.   8. Resolve conflicts from the previous freertos_hello project configuration. The Board component from the Crank Software pack includes a rewrite of pin_mux.c. Navigate to the board directory of the project and remove the pin_mux.c and pin_mux.h files.   MCUXPresso will automatically add the libraries from the runtime engine into the linker settings. In the project settings remove all the Storyboard engine libraries and plugins. To do this, right click on the project and select Properties. Remove all of the items found under C/C++ Build -> Settings -> Miscellaneous -> Other Objects.   Switch from a managed linker configuration to using the linker file included in the CMSIS pack. In the project settings, navigate to the MCU Linker -> Managed Linker Script. Uncheck the Manage Linker Script option and change the Linker script and Script path. Linker script = MIMXRT1062xxxxx_flexspi_nor.ld Script path= ${cmsis_pack_root}/CrankSoftware/iMXRT10xx/8.1.0/configuration/rt1060/ Note: The path will vary depending on where the user saved the pack.   Copy sbengine_task_pxp_template.c and sbengine_plugins_template.h from the RTE -> Graphics folder into the source folder of the project. Rename these files to remove template  from the name. The project source folder should now look like this:   Exclude the sbengine_task_pxp_template.c and sbengine_plugins_template.h files in the RTE -> Graphics folder from the build.      9. Configure and export a Model C/C++ Header from Storyboard Designer. Create a new project and name it sbengine_model. For this example, I will use a display size of 480x272, color depth RGB 565, and Freetype font manager.   Once the model has been exported, add the header file to the source directory of the project.   Note: For more information about exporting models from Storyboard Designer visit: Crank Storyboard - Exporting and Running on your Embedded Target.     10. Integrating the Storyboard Engine requires modifications to the following: FreeRTOSConfig.h file Locate this file in the source folder of the project and make the following changes: #define configFRTOS_MEMORY_SCHEME 4 #define configUSE_TIME_SLICING 0 #define configENABLE_BACKWARD_COMPATIBILITY 0 #define configTICK_RATE_HZ ((TickType_t)200) #define configUSE_NEWLIB_REENTRANT 0 To this: #define configFRTOS_MEMORY_SCHEME 3 #define configUSE_TIME_SLICING 1 #define configENABLE_BACKWARD_COMPATIBILITY 1 #define configTICK_RATE_HZ ((TickType_t)1000) #define configUSE_NEWLIB_REENTRANT 1   Preprocessor Defines Right click on the project and select Properties -> C/C++ Build -> Settings -> MCU C Compiler. Add the following defines to the “Defined symbols (-D)” pane: SKIP_SYSCLK_INIT XIP_BOOT_HEADER_DCD_ENABLE=1 GRE_TARGET_OS_freertos GRE_TARGET_CPU_cortexm7 GRE_TARGET_TOOLCHAIN_mcuxpresso GRE_FEATURE_VFS_RESOURCES   Change the SDK_DEBUGCONSOLE define from: SDK_DEBUGCONSOLE=0 to SDK_DEBUGCONSOLE=1   If you are using the gt911 touch driver, you will also need to add the following preprocessor define: SDK_I2C_BASED_COMPONENT_USED=1   Library paths. Right click on the project and select Properties -> C/C++ Build -> Settings -> MCU Linker -> Libraries.   In the Library Search path (-L) pane add: "${cmsis_pack_root}/CrankSoftware/iMXRT10xx/8.1.0/storyboard/runtime/freertos-mcuxpresso-cortexm7-swrender-DFP-obj/lib" "${cmsis_pack_root}/CrankSoftware/iMXRT10xx/8.1.0/storyboard/runtime/freertos-mcuxpresso-cortexm7-swrender-DFP-obj/plugins” Note: The path will vary depending on where the user saved the pack. This guide uses the complete configuration of the engine. Therefore, all of the following libraries need to be added in the Libraries pane (-l).  gre greal sbimage sbvfs gre-plugin-animation gre-plugin-lua gre-plugin-poly gre-plugin-circle gre-plugin-timer gre-plugin-logger gre-plugin-screen-path gre-plugin-greio gre-plugin-sbimage-soil gre-plugin-fio_vfs render-plugin-swrender logging-util greio sblua soil swrmgr swrender font-plugin-freetype sbfreetype sbpng sbz   Note: The library order matters. Add the libraries in the order listed above and click Apply and Close     11. Recall that this project was originally the freertos_hello example from the SDK. Therefore, modifications need to be made to the freertos_hello.c file to support the changes for this application. Ensure that the following headers are included: #include "board.h" #include "peripherals.h"   The define for the hello_task_priority is no longer needed and can be removed.    Place the following definitions outside of the main function: void sbengine_main_task(void *argument); void sbengine_input_task(void *argument);   Add the following two additional functions to the initialization sequence in the main() function: BOARD_InitSemcPins() BOARD_InitBootPeripherals().   Replace the hello_task code: if (xTaskCreate(hello_task, "Hello_task", configMINIMAL_STACK_SIZE + 10, NULL, hello_task_PRIORITY, NULL) != pdPASS) with: if (xTaskCreate(sbengine_main_task, "sbengine", 8192, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS)   Add the Storyboard Input handling task creation code block before the call to VTaskStartScheduler: if (xTaskCreate(sbengine_input_task, "StoryboardInput", 2048, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1); }       The source code should now look like this: /* FreeRTOS kernel includes. */   #include "FreeRTOS.h" #include "task.h" #include "queue.h" #include "timers.h"   /* Freescale includes. */ #include "fsl_device_registers.h" #include "fsl_debug_console.h" #include "pin_mux.h" #include "clock_config.h" #include "board.h" #include "peripherals.h"     /******************************************************************************* * Definitions ******************************************************************************/ void sbengine_main_task(void *argument);   void sbengine_input_task(void *argument);   /******************************************************************************* * Code ******************************************************************************/ /*! * @brief Application entry point. */ int main(void) { /* Init board hardware. */ BOARD_ConfigMPU(); BOARD_InitBootPins(); BOARD_InitSemcPins(); BOARD_InitBootPeripherals(); BOARD_InitBootClocks(); BOARD_InitDebugConsole();   if (xTaskCreate(sbengine_main_task, "sbengine", 8192, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while (1) ; }   if(xTaskCreate(sbengine_input_task, "StoryboardInput", 2048, NULL, configMAX_PRIORITIES / 2, NULL) != pdPASS) { PRINTF("Task creation failed!.\r\n"); while(1); }   vTaskStartScheduler(); for (;;) ; }     NOTE: Check that the line: #include sbengine_model.h in the sbengine_task_pxp.c  file matches the name of the exported header file from Storyboard.   The project should now build:    
View full article