Application Code Hub

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application Code Hub

Application Code Hub

The Application Code Hub (ACH) is a repository that contains software examples, code snippets, application software packs and demos developed by NXP experts.

ACH provides filter and search options to quickly find specific applications. With the support of Git capabilities, there is an easy way to import and use applications within IDE and tool environments.

The Application Code Hub is accessible directly from MCUXpresso for Visual Studio Code and MCUXpresso IDE. 

 

MCUXpresso for Visual Studio Code

To access the Application Code Hub, navigate to the QUICKSTART PANEL.

accessing-ACH-VSC.gif

 

 

You can use the search bar and the filters to help you find a specific example for your application or hardware.

ACH-project-filtering.gif

 

 

Once an example is selected the attached README file will open. This file will contain a description of the project as well as technical details. 

To import the project, the name field will automatically populate with the example project's name. Designate a location to save the project and click the Import Project(s) button.

After, confirm the project and the toolchain at the top of the window as prompted.

ACH-import-project.gif

 

 

If you are prompted to associate a repository, navigate to the PROJECTS section and add the device's SDK to the project.

To do this: right click on the project and select Configure > Associate Repository. A dropdown menu will appear on the screen. Select the device's SDK from there.

See the Getting Started guide if you have not yet imported the SDK.

ACH-asso-repo.gif

 

 

You can now build the project. Navigate to the PROJECTS section and click the build button. The project should build successfully. 

ACH-build-project.gif

 

 

MCUXpresso IDE

To access the Application Code Hub, navigate to the QUICKSTART PANEL.

ACH-MCUX-nav.gif

 

 

You'll notice that the UI is slightly different from MCUXpresso for VS Code. However, the search and filtering mechanisms are relatively similar.

ACH-MCUX-project-search.gif

 

 

To import an example project, simply click on GitHub Link and then the Next button. In the following window click Next to keep the default settings. After, select a destination to store the project and click Next. On the following window, select to import as an existing Eclipse project and click Next. Last verify the project and click Finish.

ACH-MCUX-project-import.gif

 

 

The project will be added to the Project Explorer view. To build simply select the project in the Project Explorer view and click build. 

**Note** The build button can be found in the toolbar at the top, in the Quickstart Panel, or by right-clicking on the project.

ACH-MCUX-project-build.gif

 

Labels (1)
0% helpful (0/1)
Version history
Last update:
‎09-06-2024 12:10 PM
Updated by: