Application raised an exception error: ValueError

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Application raised an exception error: ValueError

ソリューションへジャンプ
1,408件の閲覧回数
iann
Contributor III

Hi I'm trying to use V8 of the Secure Provisioning Tool to connect to our MIMXRT1160-EVK and when I select the Debug Probe under the menu Target/Debug Probe it throws an exception straight away without showing the sub menu.   Application raised an exception ValueError.png

Is there a fix for this?

Kind regards

Ian Norman

0 件の賞賛
返信
1 解決策
1,396件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Ian,

Debug Probe menu command is currently not supported for RT116x/7x. The command is supported for processors that contains debug probe selection on toolbar, like for example RW612 (see picture)

marektrmac_0-1716369198975.png

Thank you for reporting the problem, it will be fixed in next release. For now, we recommend to use the button on the toolbar instead of the command. We're sorry for inconvenience.

 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

元の投稿で解決策を見る

2 返答(返信)
1,397件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Ian,

Debug Probe menu command is currently not supported for RT116x/7x. The command is supported for processors that contains debug probe selection on toolbar, like for example RW612 (see picture)

marektrmac_0-1716369198975.png

Thank you for reporting the problem, it will be fixed in next release. For now, we recommend to use the button on the toolbar instead of the command. We're sorry for inconvenience.

 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
1,389件の閲覧回数
iann
Contributor III
Thanks for the quick response.

Ian
0 件の賞賛
返信