github repo for mcu_bootloader middleware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

github repo for mcu_bootloader middleware

Jump to solution
1,982 Views
mastupristi
Senior Contributor I

Hi,

on github is the mcux-sdk repo (https://github.com/nxp-mcuxpresso/mcux-sdk). By itself it does not contain everything that the SDK produced with the SDK builder does. Some middleware are provided as separate repo (e.g. https://github.com/nxp-mcuxpresso/mcux-sdk-middleware-sdmmc or https://github.com/nxp-mcuxpresso/mcux-sdk-middleware-usb)

I am interested in what I find in middleware/mcu_bootloader (for example of SDK 2.15.000)

mastupristi_0-1716213142191.png

I cannot find these files (e.g. bl_main.c) in any repository

Can you tell me in which repository you have stored the middleware related to mcu_bootloader?

regards

Max

0 Kudos
Reply
1 Solution
1,904 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @mastupristi 

Yes, they are the same.

Hope this will help you.

BR

Hang

 

View solution in original post

0 Kudos
Reply
3 Replies
1,917 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @mastupristi 

Sorry, the relevant code for mcu_boot is in our internal repository. Unfortunately, our mcu boot code has not been pushed to Github, so you can only refer to the code in SDK.

Hope this will help you.

BR

Hang

0 Kudos
Reply
1,909 Views
mastupristi
Senior Contributor I

Hi @Harry_Zhang 

Can you confirm that the source files I find in the SDKs in the middleware/mcu_bootloader/ directory, and which are used for examples such as evkbmimxrt1170_flashloader_cm7:

mastupristi_0-1717400818569.png

 

are the ones used to get the flashloader executable that is used by Secure Provisioning Tool

mastupristi_1-1717400850250.png

 

best regards

Max

0 Kudos
Reply
1,905 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @mastupristi 

Yes, they are the same.

Hope this will help you.

BR

Hang

 

0 Kudos
Reply