github repo for mcu_bootloader middleware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

github repo for mcu_bootloader middleware

跳至解决方案
2,103 次查看
mastupristi
Senior Contributor I

Hi,

on github is the mcux-sdk repo (https://github.com/nxp-mcuxpresso/mcux-sdk). By itself it does not contain everything that the SDK produced with the SDK builder does. Some middleware are provided as separate repo (e.g. https://github.com/nxp-mcuxpresso/mcux-sdk-middleware-sdmmc or https://github.com/nxp-mcuxpresso/mcux-sdk-middleware-usb)

I am interested in what I find in middleware/mcu_bootloader (for example of SDK 2.15.000)

mastupristi_0-1716213142191.png

I cannot find these files (e.g. bl_main.c) in any repository

Can you tell me in which repository you have stored the middleware related to mcu_bootloader?

regards

Max

0 项奖励
回复
1 解答
2,025 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @mastupristi 

Yes, they are the same.

Hope this will help you.

BR

Hang

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,038 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @mastupristi 

Sorry, the relevant code for mcu_boot is in our internal repository. Unfortunately, our mcu boot code has not been pushed to Github, so you can only refer to the code in SDK.

Hope this will help you.

BR

Hang

0 项奖励
回复
2,030 次查看
mastupristi
Senior Contributor I

Hi @Harry_Zhang 

Can you confirm that the source files I find in the SDKs in the middleware/mcu_bootloader/ directory, and which are used for examples such as evkbmimxrt1170_flashloader_cm7:

mastupristi_0-1717400818569.png

 

are the ones used to get the flashloader executable that is used by Secure Provisioning Tool

mastupristi_1-1717400850250.png

 

best regards

Max

0 项奖励
回复
2,026 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @mastupristi 

Yes, they are the same.

Hope this will help you.

BR

Hang

 

0 项奖励
回复