MCUXpressoIDE_11.9.0_2144 - JN-AN-1244 - Config Pins problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpressoIDE_11.9.0_2144 - JN-AN-1244 - Config Pins problem

1,164件の閲覧回数
Larz
Contributor III

Goodday,

 

I've imported the JN-AN-1244 into MCUXpress. I've set the MCU to JN5189 and the associated SDK is JN5189DK6 version 2.6.13.

Larz_1-1710510310973.png

 

When I go to the "Pins" configtool and select the JN-AN-1244 project I get the message:

Larz_0-1710510216483.png

 

Can I solve this?

 

0 件の賞賛
返信
2 返答(返信)

1,147件の閲覧回数
Larz
Contributor III

@Ricardo_Zamora Thank you for your reply.

I will look at the SDK\docs\wireless\Common\Connectivity Framework Reference Manual.pdf

 

Where can I find the output (output pins LED) in the JN-AN-1244 files?

For example the ExtendedColorLight has more outputs...

0 件の賞賛
返信

1,150件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. When using Connectivity applications, it is recommended to use the Connectivity Framework. Such as the "Keyboard" and "GPIO Adapter" services. So, could you please try to taking as a base these services? (Please refer to SDK\docs\wireless\Common\Connectivity Framework Reference Manual.pdf)

 

Regards,

Ricardo

0 件の賞賛
返信