In FLEXSPI_TransferHandleIRQ(), FLEXSPI_WriteBlocking(), and FLEXSPI_ReadBlocking() input/output from/to RFDR/TFDR is 1 word more than caller specifies in 'size' parameter in some cases

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In FLEXSPI_TransferHandleIRQ(), FLEXSPI_WriteBlocking(), and FLEXSPI_ReadBlocking() input/output from/to RFDR/TFDR is 1 word more than caller specifies in 'size' parameter in some cases

3,521件の閲覧回数
stephenschwartz
Contributor II

In FLEXSPI_TransferHandleIRQ(), FLEXSPI_WriteBlocking(), and FLEXSPI_ReadBlocking() input/output from/to RFDR/TFDR is  1 word more than caller specifies in 'size' parameter in certain cases

In attached image, you can see how 'size' parameter, which specifies transfer size in bytes is divided by 4 then increased by 1.

So if caller specifies:

a) Write 2 bytes : 1 word is copied into caller's buffer (Ok, as long as caller allocates in word multiples)

b) Write 3 bytes : 1 word is copied into caller's buffer (Ok, as long as caller allocates in word multiples)

c) Write 4 bytes : 2 words are copied into caller's buffer! (Buffer overflow!)

d) Write 5 bytes : 2 words are copied into caller's buffer! (Ok, as long as caller allocates in word multiples)

Does anyone know why this code does not account for case (c)? 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,326件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Stephen,

   Please tell me what the chip, board and sample code you are using?  This is useful to analysis the problem.

Waiting for your reply!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,326件の閲覧回数
stephenschwartz
Contributor II

Sorry, here is the information:

MIMXRT1052xxxxB  NEW

Build Date: 2018-07-17, Device: MIMXRT1052xxxxB

OS: Windows, Toolchain: MCUXpresso IDE

Components: (None)

SDK Version: KSDK 2.4.1 (2018-06-18)

Sample code is:

uint32_t dest[4];

flexspi_transfer_t flashXfer;

flashXfer.deviceAddress = address;
flashXfer.port = kFLEXSPI_PortA1;
flashXfer.cmdType = kFLEXSPI_Read;
flashXfer.SeqNumber = 1u;
flashXfer.seqIndex = SEQ_IDX_READ_FAST_QUAD;
flashXfer.data = (uint32_t *)dest;
flashXfer.dataSize = sizeof(dest);

FLEXSPI_TransferBlocking(FLEXSPI, &flashXfer)

0 件の賞賛
返信

3,326件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Stephen,

    I am the LPC and kinetis engineer.

    If you have the I.MX technical issue, please create the question in the I.MX area:

i.MX Processors 

  There will have have the according engineer to help you.

  Besides, next time, when you create the question post, please add the chip part number,  thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信