Azure RTOS for RT1024?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Azure RTOS for RT1024?

ソリューションへジャンプ
2,483件の閲覧回数
dmarks_ls
Senior Contributor II

I had a look at the list of supported platforms for Azure RTOS on NXP MCUs, and I see the RT1020 listed there along with the RT1010, RT1015, RT1050, RT1060, and RT1064.  Will NXP be releasing an MCUX BSP with Azure RTOS for the RT1024 variant at some point?  Seems a logical choice, given the RT1020 and RT1064 are already supported.  Thanks.

David R.

0 件の賞賛
返信
1 解決策
2,458件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi David,

There is a plan to add Azure RTOS to the SDK for the RT1024-EVK. Unfortunately, I don't have a specific date to share with you but we are going to be working to release it as soon as possible.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

元の投稿で解決策を見る

1 返信
2,459件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi David,

There is a plan to add Azure RTOS to the SDK for the RT1024-EVK. Unfortunately, I don't have a specific date to share with you but we are going to be working to release it as soon as possible.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------