Azure RTOS for RT1024?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Azure RTOS for RT1024?

跳至解决方案
2,482 次查看
dmarks_ls
Senior Contributor II

I had a look at the list of supported platforms for Azure RTOS on NXP MCUs, and I see the RT1020 listed there along with the RT1010, RT1015, RT1050, RT1060, and RT1064.  Will NXP be releasing an MCUX BSP with Azure RTOS for the RT1024 variant at some point?  Seems a logical choice, given the RT1020 and RT1064 are already supported.  Thanks.

David R.

0 项奖励
回复
1 解答
2,457 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi David,

There is a plan to add Azure RTOS to the SDK for the RT1024-EVK. Unfortunately, I don't have a specific date to share with you but we are going to be working to release it as soon as possible.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

在原帖中查看解决方案

1 回复
2,458 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi David,

There is a plan to add Azure RTOS to the SDK for the RT1024-EVK. Unfortunately, I don't have a specific date to share with you but we are going to be working to release it as soon as possible.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------