switch to bigger flash device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

switch to bigger flash device

Jump to solution
2,381 Views
gschelotto
Contributor V

Hi,

In this post Change package on MCUXpresso  it is explained how to change the device package in MCUxpresso. However how can I switch in MCUxpresso from a device to another one with the same package but bigger flash memory?

For example: MKL03Z8VFG4 to MKL03Z32VFG4

regards,

gatson

0 Kudos
Reply
1 Solution
2,299 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Gaston,

KL03 only has these three package(FG, FK, AF). You can change memory size in properties->MCU settings->Memory detail. Link file will change automatically when you compile project.

Regards,

Jing

View solution in original post

0 Kudos
Reply
2 Replies
2,300 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Gaston,

KL03 only has these three package(FG, FK, AF). You can change memory size in properties->MCU settings->Memory detail. Link file will change automatically when you compile project.

Regards,

Jing

0 Kudos
Reply
2,298 Views
gschelotto
Contributor V

Thank you Jing, it works fine.

To take effect, you also have to uncheck the Preserve memory configuration as shown

Screenshot from 2019-09-25 08-25-48.png

regards,
gaston

0 Kudos
Reply