switch to bigger flash device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

switch to bigger flash device

ソリューションへジャンプ
2,371件の閲覧回数
gschelotto
Contributor V

Hi,

In this post Change package on MCUXpresso  it is explained how to change the device package in MCUxpresso. However how can I switch in MCUxpresso from a device to another one with the same package but bigger flash memory?

For example: MKL03Z8VFG4 to MKL03Z32VFG4

regards,

gatson

0 件の賞賛
返信
1 解決策
2,289件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Gaston,

KL03 only has these three package(FG, FK, AF). You can change memory size in properties->MCU settings->Memory detail. Link file will change automatically when you compile project.

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,290件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Gaston,

KL03 only has these three package(FG, FK, AF). You can change memory size in properties->MCU settings->Memory detail. Link file will change automatically when you compile project.

Regards,

Jing

0 件の賞賛
返信
2,288件の閲覧回数
gschelotto
Contributor V

Thank you Jing, it works fine.

To take effect, you also have to uncheck the Preserve memory configuration as shown

Screenshot from 2019-09-25 08-25-48.png

regards,
gaston

0 件の賞賛
返信