MCUXpresso Config Tools - Pending Download Status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Config Tools - Pending Download Status

2,118 Views
bernardesteban
Contributor I

I can't download MK64FN1M0xxx12 (2) with MCUXpresso IDE  sdk 2.3.

I got a message like below

"NXP MCUXpresso Config Tools User,

Your recent download request is currently in a pending state due to export compliance. Please verify that your profile preferences within MCUXpresso Config Tools are detailed and accurate. You can update these preferences by logging into MCUXpresso Config Tools (http://mcuxpresso.nxp.com) and selecting preferences from the drop-down menu next to your name. If your account remains in a pending state for more than 24 hours please email [email protected] to expedite the resolution."

I tried to send an email to [email protected], but this address didn't  works!!

Incredible!

what the problem!!!

Tags (1)
0 Kudos
Reply
3 Replies

2,019 Views
BlackNight
NXP Employee
NXP Employee

I have seen reports that some strange characters in the user profile/name/account settings could trigger an 'export compliance' message. I have pinged a contact to check this, so hopefully this will be resolved. As a workaround you could create a new account, but make sure you enter only 7bit ASCII characters and no Umlaut (if this is really the problem here).

0 Kudos
Reply

2,019 Views
bernardesteban
Contributor I

Hi,

I received the authorization to download the sdk two days after this post.

At this time, just after writing this post, I could't connect again for some days, so I could't reply...

I didn't change account, and my account was not use for some months.

Thanks for your answers.

0 Kudos
Reply

2,019 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bernard Esteban ,

What about your NXP account , it is a new one ? Or a account that haven't used for a long time ?

Could you please use another NXP account to have a try ?

BR

Alice

0 Kudos
Reply