MCUXpresso 11.5.1 "Error while creating linker script"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso 11.5.1 "Error while creating linker script"

跳至解决方案
2,298 次查看
erling
Contributor III

When updating to the newly released MCUXpresso 11.5.1, my project fails to build. Please see attached error.

My setup:
Ubuntu 20.04
MCUXpresso 11.5.1
SDK 2.10.1
Board: iMXRT1170EVK

0 项奖励
回复
1 解答
2,285 次查看
erling
Contributor III

Somehow I missed multple memory regions which was reference in the managed linker script. Really wierd that these have been removed by the tool with no warning

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,286 次查看
erling
Contributor III

Somehow I missed multple memory regions which was reference in the managed linker script. Really wierd that these have been removed by the tool with no warning

 

 

0 项奖励
回复
2,290 次查看
erling
Contributor III

This seems to be a operating system related problem. I have also upgraded from Ubuntu 18.04 where everything worked. Now I get the same error using MCUXpresso 11.4.1, 11.5.0 and 11.5.1. I have tried multiple older commits of my project known to be working

0 项奖励
回复