MCUXpresso 11.5.1 "Error while creating linker script"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso 11.5.1 "Error while creating linker script"

ソリューションへジャンプ
2,294件の閲覧回数
erling
Contributor III

When updating to the newly released MCUXpresso 11.5.1, my project fails to build. Please see attached error.

My setup:
Ubuntu 20.04
MCUXpresso 11.5.1
SDK 2.10.1
Board: iMXRT1170EVK

0 件の賞賛
返信
1 解決策
2,281件の閲覧回数
erling
Contributor III

Somehow I missed multple memory regions which was reference in the managed linker script. Really wierd that these have been removed by the tool with no warning

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,282件の閲覧回数
erling
Contributor III

Somehow I missed multple memory regions which was reference in the managed linker script. Really wierd that these have been removed by the tool with no warning

 

 

0 件の賞賛
返信
2,286件の閲覧回数
erling
Contributor III

This seems to be a operating system related problem. I have also upgraded from Ubuntu 18.04 where everything worked. Now I get the same error using MCUXpresso 11.4.1, 11.5.0 and 11.5.1. I have tried multiple older commits of my project known to be working

0 件の賞賛
返信