MCUXexpresso custom command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXexpresso custom command

1,078 Views
_Ferrari_
Contributor V

Dear all,

just a question about MCUXepresso IDE.

Is it possible to add a 'custom' command to the IDE ?

For example: is it possible add a new button that clear a variable and reset the CPU ?

 

in the following picture just an axample

_Ferrari__1-1732027513833.png

 

thank you very much for your help and cooperation

regards

Tags (1)
0 Kudos
Reply
3 Replies

1,060 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @_Ferrari_ ,

Thanks for your post. In my opinion, the idea of adding a "custom" command button is not achievable. The front - end code of MCUXpresso IDE is not open source, and custom modifications are not allowed.

Best Regards,

Celeste

0 Kudos
Reply

1,055 Views
_Ferrari_
Contributor V

Ok, thank you for your answer.

Just another question:

Is there any possibility to send multiple commands (ie via console or terminal prompt) ?

just an example:

>argv=0; reset

thank you for your help and cooperation

regards

 

0 Kudos
Reply

1,045 Views
Celeste_Liu
NXP Employee
NXP Employee

I'm very sorry. I'm not certain about this question. Maybe you could have a try.

0 Kudos
Reply