MCUXexpresso custom command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXexpresso custom command

1,849件の閲覧回数
_Ferrari_
Contributor V

Dear all,

just a question about MCUXepresso IDE.

Is it possible to add a 'custom' command to the IDE ?

For example: is it possible add a new button that clear a variable and reset the CPU ?

 

in the following picture just an axample

_Ferrari__1-1732027513833.png

 

thank you very much for your help and cooperation

regards

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,831件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @_Ferrari_ ,

Thanks for your post. In my opinion, the idea of adding a "custom" command button is not achievable. The front - end code of MCUXpresso IDE is not open source, and custom modifications are not allowed.

Best Regards,

Celeste

0 件の賞賛
返信

1,826件の閲覧回数
_Ferrari_
Contributor V

Ok, thank you for your answer.

Just another question:

Is there any possibility to send multiple commands (ie via console or terminal prompt) ?

just an example:

>argv=0; reset

thank you for your help and cooperation

regards

 

0 件の賞賛
返信

1,816件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

I'm very sorry. I'm not certain about this question. Maybe you could have a try.

0 件の賞賛
返信