Installed SDK board not showing at the SDK wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installed SDK board not showing at the SDK wizard

1,941 Views
EduardoDueñas
Contributor I

I just installed MCUXpresso a couple days ago, but I'm having some problems crating a project with the SDK of frdm-kl25z. At the SDK Installer it says it is installed but nothing shows up at the SDK wizard when I try to creat a project. Any help is appreciated.

EduardoDueñas_1-1611287836899.png

EduardoDueñas_0-1611287797662.png

 

0 Kudos
Reply
4 Replies

1,936 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @EduardoDueñas 

 

Please download sdk_2.2.0_frdmKL25 from  https://mcuxpresso.nxp.com/en/welcome

danielchen_0-1611292565887.png

 

and drag the SDK.zip into MCUXpresso installed SDKs tab.

Then you will see the Frdm-kl25z when you create a new project.

 

danielchen_1-1611292690882.png

 

Regards

Daniel

 

0 Kudos
Reply

1,923 Views
EduardoDueñas
Contributor I

Hi @danielchen ,

I've alredy tried that but when I try to drag the program ask for permission but nothing happens. Also, this error is showing up some times:

EduardoDueñas_0-1611320917896.png

 

0 Kudos
Reply

1,911 Views
danielchen
NXP TechSupport
NXP TechSupport

Please make sure you have the 'administrator' right.

and the MCUXpresso IDE should be installed as administrator, you should have sufficient privileges.

 

Regards

Daniel

0 Kudos
Reply

1,904 Views
EduardoDueñas
Contributor I

Hi @danielchen,

I've alredy tried runing as administrator but the same error keep occurring. I also tried restalling but the same error keep poping up. Is there any other thing I could do?

0 Kudos
Reply