Installed SDK board not showing at the SDK wizard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installed SDK board not showing at the SDK wizard

2,101件の閲覧回数
EduardoDueñas
Contributor I

I just installed MCUXpresso a couple days ago, but I'm having some problems crating a project with the SDK of frdm-kl25z. At the SDK Installer it says it is installed but nothing shows up at the SDK wizard when I try to creat a project. Any help is appreciated.

EduardoDueñas_1-1611287836899.png

EduardoDueñas_0-1611287797662.png

 

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,096件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @EduardoDueñas 

 

Please download sdk_2.2.0_frdmKL25 from  https://mcuxpresso.nxp.com/en/welcome

danielchen_0-1611292565887.png

 

and drag the SDK.zip into MCUXpresso installed SDKs tab.

Then you will see the Frdm-kl25z when you create a new project.

 

danielchen_1-1611292690882.png

 

Regards

Daniel

 

0 件の賞賛
返信

2,083件の閲覧回数
EduardoDueñas
Contributor I

Hi @danielchen ,

I've alredy tried that but when I try to drag the program ask for permission but nothing happens. Also, this error is showing up some times:

EduardoDueñas_0-1611320917896.png

 

0 件の賞賛
返信

2,071件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Please make sure you have the 'administrator' right.

and the MCUXpresso IDE should be installed as administrator, you should have sufficient privileges.

 

Regards

Daniel

0 件の賞賛
返信

2,064件の閲覧回数
EduardoDueñas
Contributor I

Hi @danielchen,

I've alredy tried runing as administrator but the same error keep occurring. I also tried restalling but the same error keep poping up. Is there any other thing I could do?

0 件の賞賛
返信