How to enable include path in Project Explorer?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable include path in Project Explorer?

1,851件の閲覧回数
anaseem
Contributor IV

I imported LPCXpresso project to MCUXpresso IDE. 

In Project Explorer, under project name, there is Includes folder.

There are number of include paths that are disabled.  For example, following include path is disabled:

PROJ_XYZ / board_xyz / inc

I created "PROJ_XYZ / board_xyz / inc" in windows file explorer in my workspace and stored header file in this path.  But this path is still disabled in Project Explorer ? 

Regards,

0 件の賞賛
返信
2 返答(返信)

1,743件の閲覧回数
anaseem
Contributor IV

I removed disabled include paths from project properties.  Then, they disappeared from Project Explorer.  I, then re-created include paths in project properties.

0 件の賞賛
返信

1,743件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I'm not sure if I can follow what you say.

Can you post a screenshot or provide an example?

0 件の賞賛
返信