How to enable include path in Project Explorer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable include path in Project Explorer?

1,864 Views
anaseem
Contributor IV

I imported LPCXpresso project to MCUXpresso IDE. 

In Project Explorer, under project name, there is Includes folder.

There are number of include paths that are disabled.  For example, following include path is disabled:

PROJ_XYZ / board_xyz / inc

I created "PROJ_XYZ / board_xyz / inc" in windows file explorer in my workspace and stored header file in this path.  But this path is still disabled in Project Explorer ? 

Regards,

0 Kudos
Reply
2 Replies

1,756 Views
anaseem
Contributor IV

I removed disabled include paths from project properties.  Then, they disappeared from Project Explorer.  I, then re-created include paths in project properties.

0 Kudos
Reply

1,756 Views
BlackNight
NXP Employee
NXP Employee

I'm not sure if I can follow what you say.

Can you post a screenshot or provide an example?

0 Kudos
Reply