Alice,
Many thanks for your reply.
Any attempt to boot the FRDM-K66F even without pressing the reset button goes into bootloader mode and creates a "disk" on the PC. I am assuming that this means that there is a valid bootloader but a corrupt debug application. I am Correct?
I have already tried to reload the debug application by dragging the .bin file from OpenSDAv2.2_DAPLink_frdmk66f_rev0242.zip onto the BOOTLOADER disk, but a subsequent reboot still goes into bootloader mode.
I now have a 2nd FRDM-K66F, that boot correctly, both in normal mode running the tilt application and in bootloader mode,(connected to linux).
Before plugging it into Windows 10 I need to check the bootloader version to see if it is safe. How do I do that?
OpenSDA Serial and Debug Adapter|NXP says to check the bootload version, but remains silent on how to do it.
Bricking and Unbricking OpenSDA with Windows 8 and 10 - YouTube indicates that I should see a file SDA_INFO.HTM thay would say. But booting in bootloader mode on linux only shows bootload.htm that gives a link to mbed.org and a couple of zero size hidden files.
Your help is appreciated.
Regards
Tim