FreeRTOS stack backtrace not enabling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS stack backtrace not enabling

18,042件の閲覧回数
Genovation
Contributor I

I am testing FreeRTOS on an QN9090DK6 board:

IDE: MCUXpresso IDE v11.4.1 [Build 6260] [2021-09-15]

I have verified the settings for enabling backtracing in the forum posts. I am not seeing threading enabled. I am using heart_rate_sensor_freertos example project from the SDK.

All the files have been updated and running All-Stop. I reviewed the instructions in "FreeRTOS stack backtrace is disabled". I have also went through the "MCUXpresso_IDE_FreeRTOS_Debug_Guide.

What other settings do I need to verify are correct.

GDB nonstop mode disabled (using allstop mode)
FreeRTOS stack backtrace is disabled

Thanks

Chad

タグ(1)
0 件の賞賛
返信
9 返答(返信)

17,991件の閲覧回数
ErichStyger
Specialist I

what debug probe are you using? Could you share a screenshot?

Note: if using J-Link, you need to turn it on in the launch configuration settings.

And threads won't show up until you have started the scheduler.

Otherwise: does the debugger console report anything useful?

 

I hope this helps,

Erich

17,980件の閲覧回数
Genovation
Contributor I
tasks.c: attached
freeRTOSConfig.h: attached
freertos_tasks_c_additions.h: exists
 
Console output:
Probe(0): Connected&Reset. DpID: 2BA01477. CpuID: 00000C24. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Content of CoreSight Debug ROM(s):
RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)
ROM 1 E000E000: CID B105E00D PID 04000BB000 Gen SCS (type 0x0)
ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)
ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)
ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)
ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU
NXP: QN9090
DAP stride is 4096 bytes (1024 words)
Inspected v.2 On-chip Flash Memory QN9090_640K.cfx
Image 'QN9090_Internal Flash Sep 14 2021 15:10:39'
Opening flash driver QN9090_640K.cfx
Sending VECTRESET to run flash driver
Flash variant 'QN9090_Internal Flash Sep 14 2021 15:10:39' detected (646656B = 1263*512 at 0x0)
Closing flash driver QN9090_640K.cfx
Connected: was_reset=true. was_stopped=false
Awaiting telnet connection to port 3332 ...
GDB nonstop mode disabled (using allstop mode)
FreeRTOS stack backtrace is disabled
Opening flash driver QN9090_640K.cfx (already resident)
Sending VECTRESET to run flash driver
Flash variant 'QN9090_Internal Flash Sep 14 2021 15:10:39' detected (646656B = 1263*512 at 0x0)
Writing 257592 bytes to address 0x00000000 in Flash
0003E200 done  98% (254464 out of 257592)
( 98) at 0003E200: 512 bytes - 254976/257592
Sectors written: 9, unchanged: 495, total: 504
Erased/Wrote sector 0-503 with 257592 bytes in 528msec
Closing flash driver QN9090_640K.cfx
Flash Write Done
Flash Program Summary: 257592 bytes in 0.53 seconds (476.43 KB/sec)
Starting execution using system reset and halt target
Stopped (Was Reset)  [Reset from Unknown]
Stopped: Breakpoint #4
0 件の賞賛
返信

17,955件の閲覧回数
ErichStyger
Specialist I

I believe there are some symbols missing (maybe due optimization or because you are using the NXP FreeRTOS port). I maintain my own port which covers all optimization levels and compiler settings, anyway.

I recommend you might have a look at yet another article of mine, more specific to this problem:

https://mcuoneclipse.com/2017/07/27/troubleshooting-tips-for-freertos-thread-aware-debugging-in-ecli...

It describes a debug level setting you can use for the LinkServer configuration. The latest IDE somehow has the GUI for it removed somehow, but you can edit the .launch and change the setting manually:

ErichS_0-1638256698577.pngErichS_0-1638256698577.png

Then you should get a list of symbols found:

ErichS_1-1638256741129.pngErichS_1-1638256741129.png

 

I hope this helps,

Erich

 

0 件の賞賛
返信

17,937件の閲覧回数
Genovation
Contributor I

Genovation_0-1638294396345.pngGenovation_0-1638294396345.png

Genovation_1-1638294547309.pngGenovation_1-1638294547309.png

 

Looking the above, what do I need to update to make the peripherals supported since this is the example being provided? I am not sure if that is why the FreeRTOSDebugConfig does not have an address like your documentation shows.

Thanks

0 件の賞賛
返信

17,932件の閲覧回数
ErichStyger
Specialist I

As for the FreeRTOSDebugConfig:

Check that it is indeed linked with your application (and not optimized away)

ErichS_0-1638295512313.pngErichS_0-1638295512313.png

and just in case: I maintain my version here: https://github.com/ErichStyger/McuOnEclipseLibrary/blob/master/lib/FreeRTOS/Source/include/freertos_... which has been immunized against linker and compiler optimizations.

 

Keep in mind that for it there are two macros required:

ErichS_1-1638295698247.pngErichS_1-1638295698247.png

 

 

I hope this helps,

Erich

0 件の賞賛
返信

17,933件の閲覧回数
ErichStyger
Specialist I

Looking the above, what do I need to update to make the peripherals supported since this is the example being provided?

Not sure, but I guess peripherals config tools is not implemented?

You might have to check this list:

https://community.nxp.com/t5/MCUXpresso-General-Knowledge/MCUXpresso-Supported-Devices-Table/ta-p/11...

But: It would be much better if you would open a different thread for each item.

 

Erich

0 件の賞賛
返信

17,925件の閲覧回数
Genovation
Contributor I

Erich,

peripherals config tools is not implemented, in the spreadsheet line 138 is the board. QN9090DK6 is the board, Cortex-M4 I would guess falls in there. If not I can create a new thread to continue and debug this issue. 

 

Thanks

Chad

0 件の賞賛
返信

18,002件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Genovation,

I hope you are doing great.

I am not sure if I am following your case.

What are you trying to achieve? What is the example that you are running?

Could you please provide more details about the issue that you have?

Regards,

Mario

0 件の賞賛
返信

17,984件の閲覧回数
Genovation
Contributor I

I am running the heart rate sensor freetos monitor example. I am trying to see all the threads that are running to understand how the application functions.

0 件の賞賛
返信