Disabling RTCK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,391件の閲覧回数
VolcanicCheese
Contributor III

When programming via JTAG, how do you disable RTCK in MCUxpresso? Page 85 of MCUxpresso IDE User Guide indicates it is possible to disable RTCK.

0 件の賞賛
返信
1 解決策
2,382件の閲覧回数
converse
Senior Contributor V

1. Which chip are you using?

2. Why do you want to change?

Note the comment:

  • Note that RTCK (Return clock) is only used on older ARM cores (ARM7TDMI and ARM9 family) before the debug was properly decoupled from the core clock domain.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,383件の閲覧回数
converse
Senior Contributor V

1. Which chip are you using?

2. Why do you want to change?

Note the comment:

  • Note that RTCK (Return clock) is only used on older ARM cores (ARM7TDMI and ARM9 family) before the debug was properly decoupled from the core clock domain.
0 件の賞賛
返信
2,373件の閲覧回数
VolcanicCheese
Contributor III

I am using a MIMXRT 1020 board I was confused on why connecting RTCK and not TCK with a minimum pin configuration allowed the JTAG connection to work. I was wondering if it was because RTCK was enabled. Thank you!

0 件の賞賛
返信