Disabling RTCK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Disabling RTCK

跳至解决方案
2,361 次查看
VolcanicCheese
Contributor III

When programming via JTAG, how do you disable RTCK in MCUxpresso? Page 85 of MCUxpresso IDE User Guide indicates it is possible to disable RTCK.

0 项奖励
回复
1 解答
2,352 次查看
converse
Senior Contributor V

1. Which chip are you using?

2. Why do you want to change?

Note the comment:

  • Note that RTCK (Return clock) is only used on older ARM cores (ARM7TDMI and ARM9 family) before the debug was properly decoupled from the core clock domain.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,353 次查看
converse
Senior Contributor V

1. Which chip are you using?

2. Why do you want to change?

Note the comment:

  • Note that RTCK (Return clock) is only used on older ARM cores (ARM7TDMI and ARM9 family) before the debug was properly decoupled from the core clock domain.
0 项奖励
回复
2,343 次查看
VolcanicCheese
Contributor III

I am using a MIMXRT 1020 board I was confused on why connecting RTCK and not TCK with a minimum pin configuration allowed the JTAG connection to work. I was wondering if it was because RTCK was enabled. Thank you!

0 项奖励
回复