Disabling RTCK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disabling RTCK

Jump to solution
2,396 Views
VolcanicCheese
Contributor III

When programming via JTAG, how do you disable RTCK in MCUxpresso? Page 85 of MCUxpresso IDE User Guide indicates it is possible to disable RTCK.

0 Kudos
Reply
1 Solution
2,387 Views
converse
Senior Contributor V

1. Which chip are you using?

2. Why do you want to change?

Note the comment:

  • Note that RTCK (Return clock) is only used on older ARM cores (ARM7TDMI and ARM9 family) before the debug was properly decoupled from the core clock domain.

View solution in original post

0 Kudos
Reply
2 Replies
2,388 Views
converse
Senior Contributor V

1. Which chip are you using?

2. Why do you want to change?

Note the comment:

  • Note that RTCK (Return clock) is only used on older ARM cores (ARM7TDMI and ARM9 family) before the debug was properly decoupled from the core clock domain.
0 Kudos
Reply
2,378 Views
VolcanicCheese
Contributor III

I am using a MIMXRT 1020 board I was confused on why connecting RTCK and not TCK with a minimum pin configuration allowed the JTAG connection to work. I was wondering if it was because RTCK was enabled. Thank you!

0 Kudos
Reply